2015-02-25 3:08 AM
Hi, I'm using STEVAL-IDW001V1 and STEVAL-PCC018V1 boards.
I set up wifi into IBSS mode named ''ADHOC'' but I cannot detect it from the telephone or browser.I've the impression I'm not creating the ADHOC network. Where's the issue?I'm attaching data. +WIND:2:Reset+WIND:1:Poweron (141106-0950875-SPWF01S)+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.+WIND:3:Watchdog Running+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:16:BD:EC:00:B3:C5+WIND:25:WiFi Association with 'ADHOC' successful+WIND:51:WiFi Handshake Complete+WIND:24:WiFi Up:192.168.1.101# Status & Statistics:# version = 141106-0950875-SPWF01S # reset_reason = 2# conf_flag = 5# system_uptime = 103# system_sleeptime = 0# gpio_enable = 0# captiveportal = 0# wifi_state = 10# wifi_bssid = 16:BD:EC:00:B3:C5# wifi_aid = 0# wifi_channelnum = 6# wifi_sup_rate_mask = 0x003FFFCF# wifi_bas_rate_mask = 0x0000000F# wifi_chan_activity2 = 0x00000020# wifi_max_tx_power = 18# wifi_reg_country = # wifi_dtim_period = 0# wifi_sleeping = 1# wifi_num_assoc = 0# ip_ipaddr = 192.168.1.101# ip_netmask = 255.255.255.0# ip_gw = 192.168.1.1# ip_dns = 208.67.222.222# ip_sock_open = 0# ip_sockd_port = 0# free_heap = 21656# min_heap = 20312# current_time = 2342OK# Dumping All Configuration Keys:# nv_manuf = ST# nv_model = SPWF01SA1# nv_serial = 4313D25167# nv_wifi_macaddr = 00:80:E1:FF:BA:C7# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 115200# console1_hwfc = 0# console1_enabled = 1# sleep_enabled = 0# standby_enabled = 0# standby_time = 10# wifi_tx_msdu_lifetime = 0# wifi_rx_msdu_lifetime = 0# wifi_operational_mode = 0x00000011# wifi_beacon_wakeup = 1# wifi_beacon_interval = 100# wifi_listen_interval = 0# wifi_rts_threshold = 3000# wifi_ssid = 41:44:48:4F:43:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_ssid_len = 5# wifi_channelnum = 6# wifi_opr_rate_mask = 0x00003FCF# wifi_bas_rate_mask = 0x0000000F# wifi_mode = 2# wifi_auth_type = 0# wifi_atim_window = 0# wifi_powersave = 0# wifi_tx_power = 18# wifi_rssi_thresh = 0# wifi_rssi_hyst = 0# wifi_ap_idle_timeout = 120# wifi_beacon_loss_thresh = 10# wifi_priv_mode = 0# wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_key_lens = 00:00:00:00# wifi_wep_default_key = 0# wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wpa_psk_text = # ip_use_dhcp = 0# ip_use_httpd = 1# ip_mtu = 1500# ip_hostname = iwm-FF-BA-C7# ip_apdomainname = captiveportal.net# ip_ipaddr = 192.168.1.101# ip_netmask = 255.255.255.0# ip_gw = 192.168.1.1# ip_dns = 192.168.1.1# ip_http_get_recv_timeout = 3000# ip_dhcp_timeout = 20# ip_sockd_timeout = 250OK2015-02-25 8:56 AM
Pietro, I had the same problem.
To solve it I need to update the module. Try v3.3.And update it OTA. Using UART I ''brick'' the module...2015-02-25 11:48 PM
IBSS was included into FW 20140805, namely FW3.2
2015-02-26 1:08 AM
Did you set a static IP address also on smartphone?
Depending on OS, this step is mandatory.This step is not needed, for example, using iOS.2015-02-26 2:27 AM
Ok, thanks, understood. It works.
Thank you Gerardo!Bye