cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01S Test mode

jarno2
Associate II
Posted on October 18, 2016 at 14:17

Hi,

UM1695 mentions that there is a special test mode that is enabled via configuration variable ''eft_mode''. Description says ''Enable/disable the Engineering Test Functions. It is used for controlling the radio for the

certification

tests (disabled by default=0, enabled=1)''.

However I cannot find any more documentation on this. Typically in these tests we would like to select the channel and transmission and jut send some data patterns in order to measure the antenna implementation etc. How are these controlled when test mode is enabled?
1 REPLY 1
Posted on October 18, 2016 at 22:15

Hi Jarno,

there is a specific document describing how to handle test mode. Please contact your local distributor, or local ST support, to get this manual.

Regards

jerry

Hi,

UM1695 mentions that there is a special test mode that is enabled via configuration variable ''eft_mode''. Description says ''Enable/disable the Engineering Test Functions. It is used for controlling the radio for the

certification

tests (disabled by default=0, enabled=1)''.

However I cannot find any more documentation on this. Typically in these tests we would like to select the channel and transmission and jut send some data patterns in order to measure the antenna implementation etc. How are these controlled when test mode is enabled?