cancel
Showing results for 
Search instead for 
Did you mean: 

Spirit1

idris
Associate II
Posted on March 23, 2017 at 16:47

Hello everybodI have the STEVAL-IKR002Vx developmental kits and downloaded the SDK 2.0.1 and 2.2.0. I have been working on the SDK_BasicGeneric_A and B. The code compile fine in both IAR and KeilV4. However, nothing happened as indicated in the readme file inside the application folder. I noticed that the application support three evaluation boards (STEVAL-IKR002Vx,STEVAL-IDS001Vx and STEVAL-IKR001Vx ). Do I need to specify the type of kit? If yes, where can I do the sp

0 REPLIES 0