cancel
Showing results for 
Search instead for 
Did you mean: 

Spirit1 / SPSGRF receive

Lo�c Bouilly
Associate II
Posted on October 04, 2016 at 16:58

Hi,

I use the SPSGRF module in 868MHz Narrowband. I search to send packet with this configurations : 

- Fc = 869.2375MHz

- Fdev = 2.7 kHz

- Datarate = 4.8 kBit/s

- Number of channels : 0

- Spacing channel : don't care ? 

- Modulation : GFSK_BT05

So for my receiver a set : 

- Channel filters : 11,0 kHz  > (2*Fdev + datarate) ~ 10,4KHz

- SQI / PQI : Disable 

- RSSI Threshold : -20 dBm.

In this configuration I receive nothing. In my Spectrum analyzer, I see a signal when I transmit something, but receiver doesn't see : Preamble, Sync Word ...

So which parameter I miss to configure for make a reception ? Something hide ?

Or it's my transmit who is no good ? 

I think is not channel filter the problem... 

Regards,

Lo�c

 

#spirit1-rx-tx-receive-transmit
0 REPLIES 0