2018-01-06 6:06 PM
Hi,
I just got the EVAL-IDB007V1M with the spbtle-1s (based on bluenrg-1 and installed the STSW-BLUENRG1-DK (v2.5.0) on my Windows PC. The BlueNRG-1 Navigator recognizes the EVAL-IDB007V1M and I can 'Flash & Run' the basic examples and the BLE demonstration and test applications.
They seem to run on the EVAL-IDB007V1M - at least they to something when I press the buttons but I get strange results.
First, when I 'Flash & Run' the BlueNRG-1 Hello World from the basic examples I get this output:
With another terminal program it looks like this:
I expected Hello World... What's wrong?
Second problem (and more severe in my case): When I flash and run the BLE demonstration and test applications I would expect to be able to establish a connection to the EVAL-IDB007V1M from my Android smartphone. I tried to use the Apps STM32 BLE Profiles, BlueNRG and (sorry for that) nRF Connect. But I couldn't get any connection to the EVAL-IDB007V1M. I tried several demo applications, e.g. BLE Beacon.
The Apps and the BLE stuff on my smartphone works in general and I can connect to other BLE devices.
Again: What's wrong?
TIA
Wolfgang
#stsw-bluenrg1-dk #steval-idb007v1m #spbtle-1s #bluenrg-1Solved! Go to Solution.
2018-02-09 2:36 AM
Dear
wreinig
,if you're using the EVAL-IDB007V1Mboard, you have to change the setting for the 32 MHz crystal used in the SPBTLE-1S module. The BlueNRG-1 navigator is preconfigured for the EVAL-IDB007V1 board, which has another crystal (16 MHz).
Please make sure that in your project settings you use this setting:
HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ
The default configuration in all the projects that you have tried was fora 16 MHz crystal (HS_SPEED_XTAL_16MHZ)and that's why you were not able to make it work with your board.
I don't have anyEVAL-IDB007V1M board to test it myself. Please let me know if this works for you.
Best regards,
Antonio
2018-01-09 6:18 AM
Hi Wolfgang,
please keep into account that STSW-BLUENRG1-DK provides you with different applications. They define different proprietary profiles and require their specific counterpart app on the phone/tablet.
In order to test the BLE functionality, I suggest to run the BLE_SensorDemo application on your EVAL-IDB007V1M. In this case, you will need to use the BlueNRG app on your Android phone.
If you want to build and flash the BLE_SensorDemo project, the relative path within your SW package is:
Project\BLE_Examples\BLE_SensorDemo
If you want to use a pre-built binary, instead, you can find it here:
Firmware\BLE_Examples\BlueNRG-1\BLE_SensorDemo
Your current configuration for the terminal program (115200, 8N1, no flow control) is OK.
Best regards,
Antonio
2018-01-09 1:33 PM
Hi Antonio,
thank you for your fast answer. I already used 'Flash & Run' in 'BlueNRG-1 Navigator' to flash the BLE_SensorDemo. The LED DL1 is flickering a little bit but I got no BLE Connection with my smartphone (Samsung Galaxy S7) and with three different apps from different suppliers: BlueNRG, nRF Connect and BLE Scanner.To make sure BLE on my smartphone works as it should I used a BLE HRM belt which was recognized by all three apps.
With your answer I used the 'BlueNRG-1 Flasher' utility to flash the Firmware\BLE_Examples\BlueNRG-1\BLE_SensorDemo.hex file again. Same behaviour: DL1 is flickering but no BLE connection to any of the three apps (BLE HRM belt works fine)...
This is a screenshot after flashing BLE_SensorDemo.hex:
Do you have any further ideas what I could do?
best regards
Wolfgang
2018-02-09 2:36 AM
Dear
wreinig
,if you're using the EVAL-IDB007V1Mboard, you have to change the setting for the 32 MHz crystal used in the SPBTLE-1S module. The BlueNRG-1 navigator is preconfigured for the EVAL-IDB007V1 board, which has another crystal (16 MHz).
Please make sure that in your project settings you use this setting:
HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ
The default configuration in all the projects that you have tried was fora 16 MHz crystal (HS_SPEED_XTAL_16MHZ)and that's why you were not able to make it work with your board.
I don't have anyEVAL-IDB007V1M board to test it myself. Please let me know if this works for you.
Best regards,
Antonio
2018-02-12 1:33 AM
Perfect - it works!
Thank you Antonio for the very dedicated support! Because my Atollic TrueStudio 9.0.0 toolchain does not (yet) work as I expect Antonio made a 32MHZ version of BLE_SensorDemo.hex so I could test my evaluation board. Great Support!
Maybe ST should think about changing the BlueNRG-1 Navigator so it could recognize the STEVAL-IDB007V1M and flashes a 32MHZ version. This would help newcomers like me.
Now my next issue is to build a working hex file with the Atollic TrueSTUDIO 9.0.0Best regards
Wolfgang
2018-06-06 5:53 AM
i am using IAR embedded workbench and i cannot find this symbol anywhere (it was trivial in TrueSTUDIO) . Do you have some alternatives where to define it and with what scope?
Thank you,
Regards, Mitja2018-06-07 2:50 AM
Hi Mitja,
what symbol are you referring to? I'm afraid I wasn't able to fully understand your question.
Could you please add more details about your request?
Also, if this new question is unrelated to the original topic, I would kindly suggest to start a new thread as this will maximize chances of getting an answer from other community members.
Best regards,
Antonio
2018-06-07 4:34 AM
Hi Mitja,
after reading another message of yours in another thread, I understood that you were referring to preprocessor define for the crystal, i.e.
HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ
.If you're using IAR Embedded Workbench, from the menu select 'Project > Options...' and then you can define it in the 'Preprocessor' tab of the C/C++ Compiler section, as shown in the picture below.
Best regards,
Antonio
2018-06-07 4:44 AM
Thank you for a fast response! It worked like a charm!
Regards,
Mitja
2019-01-03 9:21 PM
Hi Aontonio,
i am using the EVAL-IDB007V1M board and Keil V5.
as per your previous discussion ,i change 32 Mhz and it works for "hello World" example.
here, i modify "system_bluenrg.h" file.
But BLE programs are loaded to EVAL-IDB007V1M board but the BLE Android applications not detect.
kindly give the solution...