2020-05-27 5:52 AM
I am using a STEVAL-FKI433V2 to try to create a packet sniffer. The standard on-board software is clearly capable of working with the supplied Python GUI to configure the radio and listen for packets. I have been attempting to send commands to the device over a serial port, so that I can create my own simple GUI in Python. I have managed to send and received commands to set up registers and so on, but have been unable to receive any packets.
There appears to be almost zero documentation for this CLI - there is a little documentation for the under C functions in the firmware. I'd be grateful for any advice on how to get going with this thing.
Another approach would be to write firmware. It was not clear at all what the dependencies are that need to be satisfied in order to get CLI project to build.