2024-11-05 03:09 AM - edited 2024-11-05 07:18 AM
Hello,
I'm evaluating the use of the evaluation kit and the evaluation software for the S2-LP to generate the OOK signal, In the software I can't modify the Preamble to a custom pattern, another thing is to be able to place the ID address (I can not in the software) if i enable the option to add to the frame and the last thing is if it is possible to set up two different data rate for the preamble and the rest of the frame.
Also, what is the "Length Field" in the software meant ? it is not explained, is it the length of the Address field ?
I saw in the datasheet of the S2-LP the table 52 of the preamble field selection but can someone elaborate how is that selecting the PREAMBLE_SEL for OOK the preamble would looks like?
Best regards,