cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP AFC Usage

matteo239955
Associate III
Posted on May 12, 2018 at 19:10

Hi All,

I'm evaluating the the S2-LP transceiver at 868 MHz using the Nucleo expansion board and the S2-LP DK software.

I need a clarification about the automatic frequency correction: as far as I understood from the datasheet (chapter 5.5.1), it is possible to know how far the signal that my device is receiving is from 'my' center frequency.

I have some questinos about it:

1) I see that the AFC provides the estimated frequency error through the AFC_CORR register it isn't clear to me which unit this value is... Hz? kHz? ppm?

2) How can it be related to the real frequency error?

3) In case of a continuous wave as received signal (i.e. created with a bench signal generator) this value is valid? When should i read it?

4) And how can I use it to correct the programmed center frequency accordingly?

5) Which is the range that the AFC can actually compensate?

Thanks for any reply

Mat

#s2-lp #afc #frequency-offset-correction
0 REPLIES 0