2018-12-03 06:21 AM
hello
i would like to know if it is possible to get the RSSI value of a node while it is provisioned in the mesh network. i am testing with 3 steval IDB007V2 evaluation board and i want to know how to get the RSSI value of one node A in mesh network while the both two node B,C sends they rssi value to node A.
Thank you very much.
2018-12-03 06:28 AM
any idea?
2018-12-04 07:34 PM
Hello Fahad,
Did you already refer to the discussions in this thread ?
Kindly clarify you need RSSI value of nodes before the provisioning or after the provisioning when the network is already formed ?
2018-12-06 12:05 PM
hello alok,
yes i have read this discussions thread. i need the rssi value of the nodes after the provisioning.
is it possible to get the rssi value of all nodes when the are provisioned in the mesh network?
if yes how can i do that?
Thank you
2018-12-07 12:41 AM
Hello Fahad,
We are evaluating this possibility. Give us some time to provide the feedbacks
Thanks
2018-12-09 11:18 PM
okey thank you alok.