2016-12-13 3:55 AM
I use BlueNRG-MS stack 7.2c, stackmode = 3
When connected only ONE device (mobile phone) to BlueNRG-MS everything works fine, but when startup
aci_gap_set_discoverableor
aci_gap_create_connectionfor additional second connections after some time (3 - 10 minutes) BlueNRG-MS reset by the watchdog, before it come to the event EVT_HARDWARE_ERROR=0x10 (event = 0x10, subevt_code = 0x01) and (event = 0x10, subevt_code = 0x02)
Tell me, please, what should be done to avoid reset BlueNRG-MS?
log:
[05728777] event = 0x3E (EVT_LE_META_EVENT), subevent = 0x0001 (EVT_LE_CONN_COMPLETE)
[05728779] EVT_LE_CONN_COMPLETE status = 0 ; handle = 0x0801 ; role = 1 ; interval = 30.000000, latency = 0 , supervision_timeout = 72, master_clock_accuracy = 5
[05728897] [HCI_Event_CB] event = 0xFF (EVT_VENDOR), ecode = 0x0800 (EVT_BLUE_L2CAP_CONN_UPD_RESP)
[05728897] conn_handle = 0x0801 ; code = 0x13 ; identifier = 1, result = 0
[05729257] [HCI_Event_CB] event = 0x3E (EVT_LE_META_EVENT), subevent = 0x0003 (EVT_LE_CONN_UPDATE_COMPLETE)
[05729257] EVT_LE_CONN_UPDATE_COMPLETE status = 00 ; handle = 0801, interval = 168.750000, latency = 0, supervision_timeout = 100
....
[05732794] master_devices = 1 ; slave_devices = 0
[05732800] ENTER_DISCOVERY_MODE
[05732802] aci_gap_set_discoverable() OK
....
[06198908] [HCI_Event_CB] EVT_HARDWARE_ERROR event = 0x10, evt_code = 0x01
[06202624] [HCI_Event_CB] EVT_HARDWARE_ERROR event = 0x10, evt_code = 0x01
[06204480] [HCI_Event_CB] EVT_HARDWARE_ERROR event = 0x10, evt_code = 0x01
[06204820] [HCI_Event_CB] EVT_HARDWARE_ERROR event = 0x10, evt_code = 0x01
[06205674] [HCI_Event_CB] EVT_HARDWARE_ERROR event = 0x10, evt_code = 0x02
[06220667] [HCI_Event_CB] event = 0xFF (EVT_VENDOR), ecode = 0x0001 (Firmware started properly)
[06220667] EVT_BLUE_INITIALIZED Reset caused by watchdog
#multiple-devices-simultaneously #bluenrg-ms #bleSolved! Go to Solution.
2016-12-21 3:31 AM
I found the cause of my problems. It was all in the wrong value HS_Startup_Time. When I performed XTAL_startup_TEST, which is described in
, and performed calculations obtained a value which is greater (1311 µs) than the default value (800 µs).Updated IFR and all perfectly worked.2016-12-15 1:22 AM
Found a workaround, when BlueNRG-MS sends to event EVT_HARDWARE_ERROR = 0x10 (event = 0x10, subevt_code = 0x01), I terminate the current process, with the command aci_gap_terminate_gap_procedure or aci_gap_set_non_discoverable, and run again (aci_gap_set_discoverable or aci_gap_create_connection).
The connection lasted 14 hours, which is very good, compared with 4 minutes as before.I understand that this method is not correct, it is certainly desirable to find the right way to eliminate my problems.
Please help find the right solution.2016-12-21 3:31 AM
I found the cause of my problems. It was all in the wrong value HS_Startup_Time. When I performed XTAL_startup_TEST, which is described in
, and performed calculations obtained a value which is greater (1311 µs) than the default value (800 µs).Updated IFR and all perfectly worked.