cancel
Showing results for 
Search instead for 
Did you mean: 

RE-programming SPBTLE-1S from beacon mode to BLE

rdi c.1
Associate

I bought from gilisymo a ToF sensor with integrated BLE based on SPBTLE-1S from ST. Right now the BLE is setted in beacon mode to save energy but i would like to pass to std BLE communication in a way to acquire the signal at fixed frequency. Unfortunately I am quite new on ST reprogramming, so i need some help with the code. Can I start from the examples on BlueNRG SDK?

Thanks for help

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @rdi c.1​, to the community!

The SPBTLE-1S has been obsolete since 2021, which is why no more information is available from STMicroelectronics for it.

But maybe you can find something in the depths of the never-forgetting internet that will help you?

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.