2024-05-14 2:14 AM
Hi Everyone,
I'm using BlueNRG LPS as a network co-processor with STM32L4 Nucleo Board. I'm sending 30 bytes data in every 10ms from stm32 to bluenrg LPS in Non-Block manner, and after 3000 bytes I have to send to packet end command (blocked). So there are 2 problems I'm facing -
1) In my mobile app I'm not able to receive any data,
2) When I put the breakpoint in my code then able to receive data in mobile app, but not able to receive full data, in that also able to receive packet end.
NOTE - To verify the code logic, I have run the same program flow in Bluenrg-MS and using that able to receive full data without any problem.
Function I'm using to send -
if( aci_gatt_srv_notify(connection_handle, notifyhandle+1, GATT_NOTIFICATION, 20, buffer) == BLE_STATUS_INSUFFICIENT_RESOURCES)
{
busy_count++
}
else
{
pass++
}
If not able to send as per above logic then it'll send same data again in next iteration(after 10ms).
connection parameter -
1) interval min - 6ms, interval max - 6ms, slave latency - 0, timeout - 400.
2) after calling set data length, the exchanged mtt length I received is 160.
Kindly help since I'm new to ble, Thanks in advance