2019-08-22 11:07 PM
Hi all,
Greetings of the day,
Here i am using the ST BLE Mesh app. The Hardware is stm32l152re, x-Nucleo expansion board. In the application I configured. But the modesl are not fond.
Can you pls help me..
Thanks & Regards
2019-08-23 06:00 AM
So, you are possibly using X-CUBE-BLEMESH1 project ?
The provisioning and configuration was successful ?
2019-08-26 10:49 PM
Yes, I am using X-Cube-BLEMESH1. The provisioning and configuring was successful. This problem was solved.
In addition to this, though i am able to find mesh models, in that when i am using the intensity and on/off slider, the action not appearing in the devices.(on board led is not controlled). At that time, I checked the node lib version in the vendor model, it is showing 0 as answer.
please help me..
Regards,