cancel
Showing results for 
Search instead for 
Did you mean: 

Mistake in ST3232 datasheet

David Turner
Associate
Posted on January 24, 2017 at 01:05

In the

http://www.st.com/content/ccc/resource/technical/document/datasheet/group1/40/2c/7f/62/3a/3f/47/3c/CD00002253/files/CD00002253.pdf/jcr:content/translations/en.CD00002253.pdf

, the introduction text says:

The devices require only four small 0.1 mF standard external capacitors for operation from a 3 V supply.

However, Table 9 states the capacitance value as 0.1uF, a value 1000 smaller than 0.1mF.  Please could you confirm which of these is correct (I assume 0.1uF) and update the datasheet so the values agree?

David

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Tamas Novak
Associate III
Posted on March 18, 2017 at 17:49

It is surely 100nF. I've used it a number of times and worked well.