cancel
Showing results for 
Search instead for 
Did you mean: 

LNBH26 works with DISEQC 22KHz, is it possible to work with LNB and diseqc on frequency 1MHz ?

TSour.2
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions

No, according to the DiSEqC standard, only the frequency of 22kHz is supported.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @Community member​, to the community!

You certainly know what the 22kHz is used for with DiSEqC.

Where then do you see the requirement for 1MHz?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello Sir,

Thank you for your answer.

I know that the DiSEqC protocol uses the 22 kHz signal to send its information frames, and to tell the LNB to switch between low and high band. My question is: is it possible to send the data to the LNB with a signal other than the DISEQC ?

Thank you again,

No, according to the DiSEqC standard, only the frequency of 22kHz is supported.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.