2024-07-03 1:46 AM - edited 2024-07-03 2:09 AM
Hi,
I am working on the LIS2DU12, but unfortunately it does not yet work as I expected. I do a reset and wait with the status bit of reset until it is done. The system is therefore in power-down. I then set the drdy. This immediately triggers the interrupt because the drdy bit is 1. I see that the DRDY never resets on a reset. So the reset doesn't work?
How is this possible?.