cancel
Showing results for 
Search instead for 
Did you mean: 

Is there an IBIS model for the 54AC2525 with the 3.0V/3.6V MIN/MAX process corners for worst-case analysis?

Ekko Burt
Associate

The 54AC2525 IBIS Model does not have worst-case corners set up in the model. The model is instead set to run at TYP (3.3V), MIN (2.5V), and MAX (5V). Typically, MIN and MAX are process corners are 3.0V and 3.6V covering the min/max supply. Is there a way to get an ibis model with the actual worst-case/best-case corners at 3.3V? Thanks!

1 REPLY 1

This stuff would typically come via your local sales/support office, and business contacts there.

Here, perhaps an Online Support Request directly.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..