2020-09-07 4:57 PM
Hi
Is it possible to use the STUSB4710 without the VBUS_EN_SRC switch? In such a way the the VBUS is always sourced from the supply side.
I expected this to work, but when I tried it on the STUSB4710A evaluation module, it seems it will not set any PDO's.
Any way to get it to work, or am I forced to use this switch?
The external Discharge I have understood is not mandatory, as there is an internal one, right?
This is for a DFP only application.
Thanks, Thomas Nilsson
2020-11-11 4:56 PM
no one?