2019-06-11 4:19 AM
I am newbie of ST controller.
I am working with STEVAL-BLUEMIC-1. this module contains spbtle-1s which is based on BlueNRG-1. According to the application note AN4869, firmware can update using another BlueNRG-1as central.
But I want to update firmware using mobile app. Is it possible and how?
2019-06-12 6:52 PM
Please try BlueDFU v1.0.10:
Android: https://play.google.com/store/apps/details?id=com.st.STBlueDFU
iOS: https://itunes.apple.com/it/app/st-bluedfu/id1187882971
It is tested working with STEVAL-IDB007v2 (BlueNRG-1), DK 3.1.0.
2019-06-12 9:57 PM
Hi Winfred LU
Thanks for the answer.
Along with android side I need help on Embedded side. In STEVAL-BLUEMIC-1 firmware files I am not getting any OTA service. So can I use the same service mentioned in the application note as I mentioned before or any other service is required?
2019-06-13 10:23 PM
Hi Suvarna,
Yes. Actually the same OTA service is required.
Please refer to AN4869 - The BlueNRG-1, BlueNRG-2 BLE OTA (over-the-air) firmware upgrade :
https://www.st.com/resource/en/application_note/dm00293821.pdf
Section 2.2.2, BLE application with BLE OTA service
and modify the firmware (application) accordingly.
Best Regards,
Winfred
2019-06-20 5:24 AM
Hi Winfred LU,
I go through the application note as per your suggestion and also the project source file.
I am confused between two application BLE_OTA_ResetManager and BLE_OTA_ServiceManager.
I tried with BLE_OTA_ServiceManager, I flash same example code in bluemic-1, but it didn't work.
Can you guide to add OTA service in bluemic-1?
2019-07-03 2:40 AM
hi
I am developing firmware for the OTA feature using steval-blumic-1 project folder.
In file 'OTA_btl.c' file I am getting following error
error: #5: cannot open source input file "SDK_EVAL_Config.h": No such file or directory
Where will I get this file for STEVAL-BLUEMIC-1 module?