2020-03-26 2:01 AM
Hi Community,
I need to know if it's possible to make coexist Mesh and UART on BlueNRG-2 board.
If it's possible, what files do i need to add to light mesh example and what are fonctions which helps to archive this ?
My project : I try to send data from a terminal to a BNRG-2 board with classic BLE to one Board. Then this boad will use mesh network to transmit this information (ex : 0 to turn off all LEDS and 1 to turn on)
2020-04-03 11:16 PM
Hello,
There is already Serial interface available in BLE-Mesh project. You can look at
/* Enables the serial interface using Uart */
#define ENABLE_SERIAL_INTERFACE 0
#define ENABLE_SERIAL_CONTROL 0
2020-04-08 1:42 AM
Thanks for your help. I've got a problem with the project. When i put STSW-BNRG-Mesh_1.09.000\Firmware\Projects\BlueNRG-2\Applications\Lighting_Demo in stm32CudeIDE or in Truestudio, i got problem with header files "Fatal error: hal_common.h: no such file or directory.
And i try to put those files in the project, but it's still doesn't work.
Thanks for your help