2022-02-25 08:52 AM
Does the DK example only work under IAR ARM 8.4.1?
2022-02-25 09:15 AM
Hi @BCHEN.1 ,
Ye, version from SDK release note is 8.4.1
Now, from my test I can confirm that there is no issue with recent version.
If BlueNRG-LP is not supported by your IAR version, a Add-on pack is available on SDK (Utility folder)
You may refer to below extract from SDK release note :
Hope it helps.
Regards,
Sebastien.
2022-02-25 09:49 AM
C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4
Is this the folder right for EWARM_BlueNRG-LP_Flasher_2.0.0 ?
2022-02-25 11:10 AM
Hi,
Yes : it should be the correct folder. This is your IAR installation folder.
EWARM_BlueNRG-LP_Flasher_2.0.0 is a Add-on for IAR.
It uses same folder hierarchies ad architecture as IAR installation folder.
Regards,
Sebastien.