cancel
Showing results for 
Search instead for 
Did you mean: 

IAR ARM 8.50.x can't find the processor BlueNRG-LP

BCHEN.1
Associate II

Does the DK example only work under IAR ARM 8.4.1?

3 REPLIES 3
Sebastien DENOUAL
ST Employee

Hi @BCHEN.1​ ,

Ye, version from SDK release note is 8.4.1

Now, from my test I can confirm that there is no issue with recent version.

If BlueNRG-LP is not supported by your IAR version, a Add-on pack is available on SDK (Utility folder)

You may refer to below extract from SDK release note :

0693W00000KabHQQAZ.png

Hope it helps.

Regards,

Sebastien.

BCHEN.1
Associate II

C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4

Is this the folder right for EWARM_BlueNRG-LP_Flasher_2.0.0 ?

Hi,

Yes : it should be the correct folder. This is your IAR installation folder.

EWARM_BlueNRG-LP_Flasher_2.0.0 is a Add-on for IAR.

It uses same folder hierarchies ad architecture as IAR installation folder.

Regards,

Sebastien.