cancel
Showing results for 
Search instead for 
Did you mean: 

I2C communication error with STUSB4500

Andras
Associate

Hi Community,

I have a STREF-SCS001V1 board and I try to create communication with STUSB4500 IC via I2C, but there is no response. I tried to sweep addresses from 0x00 to 0xFF but there is not hit for any address. Also I tried 0x50 and 0x51 alone but does not work either.

My setup is:

  • The board is powered from USB-C from a Mac wall adapter
  • I connect the I2C with SCL/SDA pulled up to +3V3, ground connected
  • I create the communication from a python script from Pycharm

I checked the I2C frames with scope and all seems correct, it puts out what I program so I do not understand what happens. Can it be that the STUSB4500 chip is locked for some reason? I have no other guess.

Thanks,

Andras

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0