2021-04-28 12:35 PM
I want to use hyperflash (S26KS512 or S26KL512) with stm32h723zet6 microcontroller.
The memory has "Phase Shifted Clock" pins.
What should I do with them? Connect to GND or VCC or Not Connected?
Hyperbus interface (stm32) support 1.8v?
2021-06-01 9:50 PM
Should I use a 1.8 volt power supply (VDD 1.8V)?
Can I use 3.3 volt(VDD 3.3V) power supply with 1.8v hyperbus?
2021-06-01 11:50 PM
Seems like entirely the wrong subforum to post this.
The KL model looks to be the 2.7 - 3.6V part, I certainly wouldn't be using the 1.8V part at voltages exceeding the maximums specified.