cancel
Showing results for 
Search instead for 
Did you mean: 

How can I load the binary file via USB?

MMerc.1
Senior

Hi,

I want to use an USB device in order to load the .elf file via USB on STM32F746.

How can I do this?

Best Regards

12 REPLIES 12
MMerc.1
Senior

Any ideas ?

XTorr.1
Associate II

this convert .BIN to DFU

use DfuSe --> "dfu file manager"

C:\Program Files (x86)\STMicroelectronics\Software\DfuSe v3.0.6\Bin\DfuFileMgr.exe

option one

multiBin

select file.

add to list

ok

Generate

XTorr.1
Associate II

in my case STM32F207IGT

compiler project in release mode. --> .bin

"Dfu file manager"

08000000 (in map file show adress: FLASH           0x0000000008000000 0x0000000000100000 xr

DF11 produc ID (in DfuseDemo show show this information)

2200 version  (in DfuseDemo show show this information)   

DfuSeDemo --> in case STM32F207IGT: on the user board it only changes position SW boot0 [boot/Run]