‎2022-06-28 04:00 AM
What I want to do is quite simple in theory :
1) Load the BLE Beacon application from the BlueNRG-LP Development Kit (DK) on the first BlueNRG-LP board and run
2) Verify with an Android BLE Scanner Phone app that the BLE Beacon app on the BlueNRG-LP is periodically updating (like RSSI values)
3) Start from some application in the DK (say the BLE_RC_LongRange project)
4) Modify this project source code to perform a passive scan on the 1M PHY (neutering connections as I am not interested in those for this experiment)
5) Override the hci_le_extended_advertising_report_event and hci_le_advertising_report_event callbacks recompile and place them in the project with breakpoints and run on the second BlueNRG-LP board
Result: Not hitting callback breakpoints on second board which I would expect because first board is constantly beaconing.
I left out a lot of details to keep the question as concise as I can.
My question is: Am I going about this the proper way and if not can you suggest two DK sample apps I can start from so I can slay this?
Thanks for any guidance..
JRW
‎2022-08-03 04:49 AM
You are welcome. The "black hole" effect in the Community can be a bit unsettling. Sometimes, I just need somebody to commiserate with ....
‎2022-08-03 06:14 AM
I couldn't agree with you more