cancel
Showing results for 
Search instead for 
Did you mean: 

Hi STM, i'm planning in using an BLE module as an GATT client and use AT commands with an STM32F407. Could someone tell me if i can use an Blue NRG module? I

LMuni.1
Associate

I know there is an Application Command interface for the BLUENRG-M2. Is it similar to AT commands? I did not foud anything about AT commands in their documentation

1 REPLY 1
Winfred LU
ST Employee

It is because Application Command Interface (ACI) would be more like Host Controller Interface (HCI).

In fact, it is an extending of HCI, with vendor specific HCI commands and vendor specific HCI events.