cancel
Showing results for 
Search instead for 
Did you mean: 

Hello I am interested in an ST-Link cable connector which requires the least amount of pins from a JTAG connector can you please reccomend something please ?

LMyle.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

For ST-LINK V2, JTAG cable is used for connection to a standard JTAG 20-pin pitch 2.54 mm connector, and for ST-LINK-V3, Flat cables STDC14 to MIPI10 / STDC14 / MIPI20 (connectors with 1.27 mm pitch)

You can refer to AN4989 for more details

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL