2023-01-25 9:01 AM
I connected:
SIM7000E -> ST4SIM-200M
PIN 30 SIM_VDD -> VCC
PIN 31 SIM_DATA -> I/O
PIN 32 SIM_CLK -> CLK
PIN 33 SIM_RST -> RST
When I send the AT+CCID command it returns: "+CME ERROR: SIM not inserted"
The same command with a standard plastic SIM card works and returns the right card's ICCID.
Did I make the wrong connections? Do I have to do something about RESET denied?
Thank you
2023-01-25 3:10 PM
Ok, it's work...
Maybe whena I solder the chip at 480C° I burned it.
Now I used a new chip and skipped it at 280C° and it work.
Thanks
2024-04-16 5:14 AM
Hi I'm having very similar issues with my sim7600G and ST4SIM-200M. Was there any other connections you had to add, like the 20K pullup between SIM_VCC and SIM_IO? It recommends this pullup on the ST4SIM-200M datasheet, though I do not know if it's strictly required with SIMCOMM modules.DId you add much (if any) capacitance to the SIM_VCC line?
After I seen your post about the reflow temperature, I replaced the esim and used low melt solder, it's still responding with "+CME ERROR: SIM not inserted".