2021-01-22 12:14 AM
Hi, I use a X-NUCLEO-BNRG2A1 with a NUCLEO-L476RG .
I want to transfer a file (a driver) with the BLE, is it possible?
Or does the X-NUCLEO-BNRG2A1 allow the use of bluetooth BR / EDR to transmit files with the OPP profile?
2021-01-25 5:44 PM
It is possible to transfer a file over BLE. Transferring data is one of the main functions of BLE actually.
X-NUCLEO-BNRG2A1 (BlueNRG-M2SP based) is a BLE only expansion board, which means it doesn't support BR/EDR nor classic profiles such as OPP.