cancel
Showing results for 
Search instead for 
Did you mean: 

driver and application built for BlueNRG

hui
Associate II
Posted on January 19, 2015 at 22:31

Hi-

I am new to BlueNRG and supposed to created driver and application for it. The chip is used to collect sensor data remotely on my custom board that is running MQX RTOS and already comes with SPI driver. My question is, where should I start from? Or, is there sample code with less HW coupled that I can port over to my project?

Thanks!

Hui

#bluenrg-sample-code-driver
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on January 21, 2015 at 11:37

Hi Hui,

At the following link:

http://www.st.com/web/en/catalog/tools/PF259737

you can download the sw package that contains the GUI, firmware example (SensorDemo, Chat, etcc), Documentation, etcc.

In add at the following link:

http://www.st.com/web/catalog/sense_power/FM1968/CL1976/SC1898/PF258646?ecmp=pf258646_link_emf_jan2014&sc=bluenrg

#

you can download the Application Note AN4494: Bringing up the BlueNRG  that explain you how to configure the BlueNRG Device on your customer board.

Regards,

Graziella