2015-01-19 1:31 PM
Hi-
I am new to BlueNRG and supposed to created driver and application for it. The chip is used to collect sensor data remotely on my custom board that is running MQX RTOS and already comes with SPI driver. My question is, where should I start from? Or, is there sample code with less HW coupled that I can port over to my project? Thanks! Hui #bluenrg-sample-code-driver2015-01-21 2:37 AM
Hi Hui,
At the following link:
http://www.st.com/web/en/catalog/tools/PF259737
you can download the sw package that contains the GUI, firmware example (SensorDemo, Chat, etcc), Documentation, etcc.In add at the following link:
# you can download the Application Note AN4494: Bringing up the BlueNRG that explain you how to configure the BlueNRG Device on your customer board.Regards,
Graziella