2022-04-08 05:11 PM
The databrief for this kit doesn't explicitly state that it comes with an antenna, just "SMA female connector".
Can someone confirm if it ships with an antenna? If not, any suggestions for one that fits it?
Solved! Go to Solution.
2022-04-11 02:23 AM
Welcome, @EWert.1, to the community!
Yes, a magnetically mountable antenna is bundled with the X-NUCLEO-GNSS1A1 as you can also find in UM2334, which is part of the software package X-CUBE-GNSS1.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2022-04-11 02:23 AM
Welcome, @EWert.1, to the community!
Yes, a magnetically mountable antenna is bundled with the X-NUCLEO-GNSS1A1 as you can also find in UM2334, which is part of the software package X-CUBE-GNSS1.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter