2023-05-05 1:58 AM
Dear all,
I am using a BlueNRG-LPS in my current project. Stack Library 3.1a is used.
The device works as a peripheral.
It works fine to establish a connection to the peripheral, but I am facing an issue to disconnect.
There are several reasons that our custom application on the peripheral device has to terminate a connection.
Ther is a function to do so:
/**
* @brief Command the controller to terminate the connection. A @ref
* hci_disconnection_complete_event event will be generated when the link
* is disconnected. It is important to leave an 100 ms blank window
* before sending any new command (including system hardware reset),
* since immediately after @ref hci_disconnection_complete_event event,
* system could save important information in non volatile memory.
* @param Connection_Handle Connection handle that identifies the connection.
* Values:
* - 0x0000 ... 0x0EFF
* @param Reason The reason for ending the connection.
* Values:
* - 0x05: Authentication Failure
* - 0x13: Remote User Terminated Connection
* - 0x14: Remote Device Terminated Connection due to Low Resources
* - 0x15: Remote Device Terminated Connection due to Power Off
* - 0x1A: Unsupported Remote Feature
* - 0x3B: Unacceptable Connection Parameters
* @retval Value indicating success or error code.
*/
tBleStatus aci_gap_terminate(uint16_t Connection_Handle,
uint8_t Reason);
The reasons 0x05 or 0x13 both work fine. But I always get an error when reason 0x14 (low resources) is used.
The Error code I get in this case is 0x12 which means "invalid parameter".
Any ideas what could be wrong?