cancel
Showing results for 
Search instead for 
Did you mean: 

Direction controll pin voltage level of 54AC164245

kuhelika bera
Associate
Posted on July 31, 2017 at 10:31

What should be the voltage level for dir pin of 54AC164245 for logic high when it is used as bi-directional level translator.

It is not clearly stated in datasheet. Should it be 3.3V or 5V ? Please clarify.

1 REPLY 1
Brian Kling
Senior III
Posted on August 03, 2017 at 17:56

Sorry for the delay; unfortunately we don't currently have a resource in the community for the aerospace group. Therefore, can you log a support ticket at

https://my.st.com/tmtrack/tmtrack.dll?ProjectPage&Template=submit&ProjectId=9&TableId=1011