cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting BLUENRG-M2SA to a Raspberry Pi

bifftannen
Associate

Hi,

I want to conenct the BLUENRG-M2SA to a Raspberry Pi. This needs to be done through the USB connector.

Can I use a USB-to-UART IC to connect to the UART pins of the BLUENRG-M2SA and then flash the software using this?

Also, do I need to connect the reset pin to the Raspberry Pi, when I flash the software.

Thanks.

0 REPLIES 0