2025-06-04 4:14 PM
I want to connect the AD7605-4BSTZ ADC (operating from +10V to -10V) with the STM32H743. I plan to use a parallel connection for 16 bits to achieve high accuracy, and I also want to utilize DMA. I need to configure the microcontroller in STM Cube IDE to use this connection. Additionally, I would like to simulate the setup before starting the manufacturing process.