Comms between 2 x IDW01M1 boards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-19 9:24 AM
Hi,
I am working on the IDW01M1 wifi module. To-date I have been able to connect 2 of these modules to a common server and send commands between them via the server. I am now trying to connect directly between the modules without the need for the server. I have been able to create an adhoc network but I am unsure about how to setup the boards as both clients and servers. I have searched for any setup information for communicating between 2 IDW01M1 boards and have not been successful.
Could anybody point me in the right direction as to how I could get communications going directly between 2 boards.Regards,
COD#wifi-spwf01sa #idw01m1- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-10-23 9:10 AM
I have one board setup as a server and the other board setup as a client and when I try to connect I am receiving 'WIND: 74 Rejected found Network'. I was able to connect to my android phone earlier using this method.
# Status & Statistics:
# version = 170111-665d284-SPWF01S# reset_reason = 2# conf_flag = 5# system_uptime = 149# system_sleeptime = 0# gpio_enable = 0# captiveportal = 0# wifi_state = 5# wifi_bssid = 00:00:00:00:00:00# wifi_aid = 0# wifi_channelnum = 0# wifi_sup_rate_mask = 0x003FFFCF# wifi_bas_rate_mask = 0x0000000F# wifi_chan_activity2 = 0x00001FFF# wifi_max_tx_power = 12# wifi_gf_mode = 0# wifi_regccountry DE# wifi_dtim_period = 1# wifi_sleeping = 0# wifi_num_assoc = 0# ip_ipaddr = 0.0.0.0# ip_netmask = 0.0.0.0# ip_gw = 0.0.0.0# ip_dns = 0.0.0.0# ip_dns2 = 0.0.0.0# ip_sock_open = 0# ip_sockd_port = 0# free_heap =20024# min_heap = 19784# current_time = 606=================================================
# Dumping All Configuration Keys:
# nv_manuf = STM# nv_model = SPWF01SA11# nv_serial = value# nv_wifi_macaddr = 00:80:E1:B9:77:BD# etf_mode = 0# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 115200# console1_hwfc = 1# console1_enabled = 1# console1_delimiter = 0x000000CC# onsole1_errs = 1# sleep_enabled = 0# standby_enabled = 0# standby_time = 10# wifi_tx_msdu_lifetime = 0# wifi_rx_msdu_lifetime = 0# wifi_operational_mode = 0x00000011# wifi_beacon_wakeup = 1# wifi_beacon_interval== 100 wifi_listen_interval = 0# wifi_rts_threshold = 3000# wifi_ssid = 43:54:41:43:53:5F:41:64:68:6F:63:5F:45:72:6E:65:73:74:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_ssid_len = 18# wifi_txfail_thresh = 5# wifi_dtim_period =1# wifi_add_tim_ie = 1# wifi_ht_mode = 0# wifi_channelnum = 1# wifi_opr_rate_mask = 0x00003FCF# wifi_bas_rate_mask = 0x0000000F# wifi_mode = 1# wifi_region = 1# wifi_auth_type = 0# wifi_atim_window = 0# wifi_powersave= 0# wifi_tx_power = 12# wifi_rssi_thresh = 0# wifi_rssi_hyst = 0# wifi_ap_idle_timeout = 120# wifi_beacon_loss_thresh = 10# wifi_priv_mode = 2# wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wiii_wep_eys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_key_lens = 00:00:00:00 wifi_ep_default_key = 0# wifi_wpa_psk_raw = 99:26:E4:84:73:1C:58:8E:1D:17:B5:08:DF:E8:B2:92:E2:64:12:43:9D:17:37:E9:57:68:21:15:C8:7A:E3:DD# wifi_wpa_psk_text = T1tpfctaahn# ip_use_dhcp = 1# ip_use_httpd = 1# ip_mtu = 1500# ip_hostame = iwm-B9-77-BD# ip_apdomainname = captiveportal.net# ip_apredirect = firstset.html# ip_ipaddr = 192.168.0.123# ip_netmask = 255.255.255.0# ip_gw = 192.168.0.1# ip_dns = 192.168.0.1# ip_http_get_recv_timeout = 3000# ip_ait_timeout = 12000# ip_dhcp_timeout = 20# ip_sockd_timeout = 250# ip_dhcp_lease_time = 120# ip_dns_mode = 0# ip_use_cgis = 0x0000000F# ip_use_ssis = 0x0000000F# ip_use_decoder = 0x00000000# ip_block_pings = 0Thanks,
cod