cancel
Showing results for 
Search instead for 
Did you mean: 

CHIP ANTENNA with S2-LPQTR for 433MHz RX

Posted on April 19, 2018 at 11:10

Hi All,

We are looking for a Chip Antenna for S2-LPQTR. We need 433MHz RX with a 100-200m range requirement. We are using

S2-LPQTR

 since it drains only a low current and it has only a small form factor. We need a chip antenna which can be used for this application. I am looking for chip antenna since we have space constraint reason. We don't have any expertize in antenna designing. So we need your suggestions & recommendations for designing the 433MHz RX with S2-LP. Please provide reference schematics of S2-LP with the chip antenna if there is any.

Any help will be greatly appreciated. Thanks in Advance.

Best Regards,

Krishnaprabha S Naik

#s2-lp #s2-lpqtr
0 REPLIES 0