2022-04-18 4:58 AM
2022-04-18 6:20 AM
2022-04-18 6:38 AM
I don't have that board, but some options for many STM boards:
1) If you have the 14pin STLINK connection then plug in an STLink and it may also have a UART connection which will automatically show up on a PC via the STLINK USB.
2) If you have a spare pins with UART (Tx, Rx) then you can use an adapter cable like FTDI TTL-232R-3V3, which will give you a USB connection to PC TerraTerm/Coolterm/others.
3) If the STM32 has a USB port then you can wire it directly to PC and by running appropriate code on STM32 emulate a COM port to the PC. (Look at my posting history for examples). *If this is to be used by customers add appropriate ESD protection circuitry to USB, if only for lab testing you can be very minimal.
Paul
2022-04-18 6:44 AM
If you are aiming for wireless data then possibly:
1) Bluetooth
2) BLE (Lower Power)
3) Check out MBED website https://os.mbed.com/ Years since I played with that but "over the air" firmware updates (FOTA) and data was a nice feature.
Paul
2022-04-18 10:16 PM
Thank you very much Paul.
I will try doing what you suggested.