2020-11-03 10:55 PM
We have designed a custom board using BlueNRG-2 and are now working on developing applications on the same. However, the Evaluation Tool Software only consist of BlueNRG-1, BlueNRG-2 DK SW package, which we understand is the package for Development kits. Is Similarly, neither the GUI nor the Navigator can work with custom boards. there no support or resources available for standalone BlueNRG2?
Kindly provide some guidance at the earliest.
Regards
2020-11-05 6:39 PM
The DK works for customized BlueNRG-2 boards too.