cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG Set Advertising Data

dimitar
Associate II
Posted on December 10, 2014 at 07:41

Hi,

I'm trying to set the advertising data and make it advertise, but the client doesn't detect any of the data.

Here are the command that I use:

HCI_LE_Set_Advertizing_Parameters

HCI_LE_Set_Random_Address

HCI_LE_Set_Advertizing_Data

HCI_LE_Set_Advertize_Enable

What am I missing?

Thanks
1 REPLY 1
Posted on December 11, 2014 at 10:47

Hi Dimitar,

Using the commands below, the client device should be able to see the device.

Anyway, could you tell me which parameters are used?

Regards,

Graziella