2021-11-26 11:01 AM
I need the BLUENRG-M2SP schematic to qualify the application with the STmicro electronics library.
I need to configure the mode of the AC/DC converter. The spec sheet is not documented enough. With the schematics, I will understand what I need.
2021-12-01 1:12 AM
Hello,
I would usggest to look at BlueNRG-2 datasheet.
BlueNRG-2 is the SOC embedded inside BlueNRG-M2.
Pins 1 and 2 of BlueNRG-M2 module are connected directly to pin 15 and 16 of BlueNRG-232 inside the module.
BlueNRG-2 datasheet is providing detail on ADC use.
Regards
Laurent
2021-12-02 3:29 PM
Hey Laurent,
Thanks for your kind response, this is helping us :)