2015-01-08 02:25 PM
Hi,
I have a STEVAL-IDB002V1.Which image file to use to update the BlueNRG stack to 6.4. bluenrg_6_4_Mode_2-16MHz-XO32K. img orbluenrg_6_4_Mode_2-16MHz-XO32K_HCI.imgWhat is the difference between them?Thanks2015-01-09 09:46 AM
I thought that I understood the ST documentation to describe that the *_HCI.img builds (e.g. bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img) as being built to support ONLY the officially specified HCI commands (i.e. no vendor specific ACI) in order to be used for conformance testing.
2015-01-21 07:26 AM
Hi Dimitar,
to update the BlueNRG stack to version 6.4 you have to use the firmware image ''bluenrg_6_4_Mode_2-16MHz-XO32K.img'', in fact as Code has said, the version *_HCI.img supports only the HCI APIs (no GAP APIs) and it is provided only for certification. Regards, GraziellaHi,
I have a STEVAL-IDB002V1. Which image file to use to update the BlueNRG stack to 6.4. bluenrg_6_4_Mode_2-16MHz-XO32K. img or bluenrg_6_4_Mode_2-16MHz-XO32K_HCI.img What is the difference between them? Thanks