cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-2 manual/register describtion

KTarc
Associate II

Is there any manual for BlueNRG-2 where I can find the register describtion? the point is to use UART but without HAL driver. I mean document like other STM32 MCU have.

BR KWT

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
ChahinezC
Lead

Hello @KTarc​,

I am not a BlueNRG expert, but the BlueNRG-2 datasheet describes the registers and should help you.

You can find other documents in the "Documentation" section of the ST official website.

Chahinez.

KTarc
Associate II

Those documents do not provide needed data.

MMate.3
Associate II

I also cant find more information on the bluenrg1/2 chips. To be specific I need to use BlueNRG2 as network controller with host in external SoC. However the provided DTM firmware is not what I need. The DTM expose only LE part of some commands and therefore is not suitable for all type of scenarios.

It has something to do with the LL_MODE *** how is the DTM build. More documentation is needed from the ST.