2020-06-03 9:59 AM
Hi guys,
I have STEVAL IDB008V2 DK board and install BlueNRG-2 Navigator. The board appears in device manager as a VCP10, also recognized by BlueNRG-2 Navigator (meaning flash and run is activated). However, when I try to program it using any pre-build examples in BlueNRG-2 Navigator by pressing flash and run, after a few seconds, the BlueNRG-2 Navigator is closed/disappeared and nothing happen!!
I also try to program it using GUI by pressing putting the board in DFU mode, but also doesn't help!
Any idea would be highly appreciated in advance!
Regards
Edmond