2017-02-23 4:00 AM
Hi ST,
I am working with the BlueNRG-1 using STEVAL_IDB and i have few questions please:1- When i program some ST BLE via using Navigatorv2.3.0, the main code not the BLE stack, where it saved? in the main MCU or the NRG-1?2- I want to combine the NRG-1 with TI sub1-GHZ cc1310(Backward compatibility), so i have few questions in this area: 2.1 - Where the code that related to the BLE must run? on the cc1310 or NRG-1? 2.2 - Did it possible to configure and send commands to the NRG-1 via other MCU? if yes i would be happy if you share some example, reference ...3- Did there is some tool develop/debug with the
BlueNRG-1 code example, and it's free?
4- What is the best IDE that you recommended to work with the BlueNRG-1?
Thanks.
#bluenrg-12017-02-23 7:21 AM
Hi,
You may refer to the User manualsand related Tools/softwarein the
.The BlueNRG GUI is available in
/external-link.jspa?url=https%3A%2F%2Fmy.st.com%2Fcontent%2Fmy_st_com%2Fen%2Fproducts%2Fembedded-software%2Fwireless-connectivity-software%2Fstsw-bnrgui.license%3D1487062354html
.Hope this helps you.
Regards
Imen
2017-03-08 3:00 AM
Thanks
Imen D for responding,
After looking to the references that you advice to me, i have few question please:
As i mentioned before, we want to use TI cc1310 for SUB1-GHz and the NRG-1 for BLE, there is 2 ways (that i know about):
1- Connect the NRG-1 to the cc1310 via SPI and send ACI commands.
2- Set the NRG-1 as a Stand Alone, and share some memory between the cc1310 and the NRG-1 for logic's and others...
Q1: did the ACI commands have full control of the BLE stack as the Stand Alone?
Q2: What is the best way, the first way or the second?
Q3: Did there is another way that o didn't mentioned?
Any other advice in this topic will be welcome.