cancel
Showing results for 
Search instead for 
Did you mean: 

B-L072Z-LRWAN1 - StartUp RF test

JNone.1
Associate

Hi and thanks for this community, it is really useful to find answers and how-to stuff... really appreciate.

Recently I bought a couple of B_L072Z-LRWAN1, right now, just to do a quick RF test.I need it before anything else. The firmware loaded allow to do it quickly, a ping-pong play between two boards, which is nice. But I am facing some questions...

I have not installed the I-Cube and the LRWan pack yet. Next step. As I said, just quick RF test.

Just, I need to do some changes in RF settings to check it, frequency, SF, BW... this is just for Node to Node test.

I see some documents regarding AT commands. I have the board connected thru ST-Link and virtual com, and I am able to see the ping-pong messages, but no answer from any AT Command...

Someone could help how to start with it?

Many thanks in advance

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0