cancel
Showing results for 
Search instead for 
Did you mean: 

After running example, the module can't be programmed again

Adam0
Associate

Hello, has anyone had such a problem?

After flashing and running the example (BLE_OTA_ServiceManager), the module (BlueNRG-M2SA) can no longer be programmed via swd ((module still alive).

bluenrg.jpg

 

RF Flasher Utility 4.5

 

******MASS ERASE OPERATION******

14:35:14.540: Waiting device to Mass Erase memory (device connected by ST-Link) -> FAILED. (It's not possible to connect to the device)

bluenrg_flash.jpg

APP: BlueNRG-1_2 DK 3.2.3\Project\BLE_Examples\BLE_OTA_ServiceManager

 

Thanks in advance for the answers!

 

2 REPLIES 2
Roger SHIVELY
ST Employee

Hello @Adam0 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Roger

 

Adam0
Associate

The solution to the problem was to use the 'BlueNRG-1 ST-LINK Utility' flasher. Settings as in the picture:
flasher_NRG.jpg

 

The RF-Flasher Utility application could not cope with the stuck module (No extended programming options):
flasher_Utility.jpg