2024-09-24 05:40 AM - edited 2024-09-24 05:52 AM
Hello, has anyone had such a problem?
After flashing and running the example (BLE_OTA_ServiceManager), the module (BlueNRG-M2SA) can no longer be programmed via swd ((module still alive).
RF Flasher Utility 4.5
******MASS ERASE OPERATION******
14:35:14.540: Waiting device to Mass Erase memory (device connected by ST-Link) -> FAILED. (It's not possible to connect to the device)
APP: BlueNRG-1_2 DK 3.2.3\Project\BLE_Examples\BLE_OTA_ServiceManager
Thanks in advance for the answers!
2024-09-26 11:13 AM
Hello @Adam0
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger
2024-09-30 04:23 AM
The solution to the problem was to use the 'BlueNRG-1 ST-LINK Utility' flasher. Settings as in the picture:
The RF-Flasher Utility application could not cope with the stuck module (No extended programming options):